DWP 10
Original instructions for use
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Symbols
Symbols in this documentationRead the operating instructions before use. |
|
Instructions for use and other useful information |
|
Dealing with recyclable materials |
Read the operating instructions |
|
Maximum operating pressure |
|
Filling quantity |
|
CE test number |
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationWater supply unit DWP 10 Generation: 01 Serial number:
Safety
Safety instructions
- Never tamper with or modify the product in any way.
- Never tamper with or modify the safety valve in any way.
- Children and minors may not use this product.
- Never fill hydrogen peroxide or other oxygen emitting media.
- On contact with materials of the water pressure tank, explosive pressure increases are possible.
- Check to ensure that the water supply unit does not exceed the maximum operating temperature.
- If it exceeds the maximum operating temperature, explosive pressure increases are possible.
- Watch the pressure gage at all times during pumping in order not to exceed the max. operating pressure.
- Empty the tank daily after use.
- Never leave residues in the tank.
- Store the product in a dry place where it cannot be accessed by children or unauthorized persons.
Description
Product overview
- Tank
- Filling quantity display
- Locating pin
- Pressure gage
- Safety valve
- Pump
- Hose plug-in nipple with ball valve
- Hose
- Hose plug-in nipple
- Drain opening
Intended use
The product described here is a water pressure tank for distributing coolants and flushing liquids on drilling rigs, concrete saws or angle grinders. Water is generally used for this purpose.
Possible misuse
This product is not suitable for:- Flammable liquids
- Hydrogen peroxide and similar oxygen emitting media
- Caustic substances (certain disinfectants and impregnating agents, acids, alkaline solutions)
- Liquids containing ammonia
- Solvents and liquids containing solvents
- Viscous or sticky liquids or those that form residues (paints, grease)
- Use in food sector
- With external pressure sources
- For warehousing and storage of liquids
- As an eye wash
Items supplied
Tank with pump, hose with connectors, instructions for use.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group | USA: www.hilti.com
Technical data
The tank material consists of steel with a polyester coating.Tare weight |
5.2 kg |
Total content |
13 ℓ |
Maximum filling quantity |
10 ℓ |
Technical residual quantity |
0.03 ℓ |
Maximum operating pressure |
6 bar |
Maximum operating temperature |
40 ℃ |
Preparations at the workplace
Assembling water supply unit
- Check whether the tank, pump and hose are undamaged before assembly.
- Connect the hose on the drain opening [1].
- Pump up the empty water supply unit to 2 bar [2].
- The pressure must not drop by more than 0.5 bar within 30 minutes!
- The pressure must not drop by more than 0.5 bar within 30 minutes!
- Pull the red button of the safety valve for checking [3].
- The pressure must be released.
- The pressure must be released.
Fill water supply unit
- Fill the water into the tank [1].
- Check the fill level on the hose [2].
- Route the transparent hose several times on the tank from top to bottom [3].
- The liquid level in the hose and tank are equalized. The liquid level visible in the hose then matches the filling level in the tank, which you can read off on the scale.
- The liquid level in the hose and tank are equalized. The liquid level visible in the hose then matches the filling level in the tank, which you can read off on the scale.
Preparing water supply unit
- Screw the pump into the tank [1].
- Press the pump handle downward and turn it clockwise [2].
- The pump handle has been released.
- The pump handle has been released.
- Generate a pressure of approx. 2 bar in the tank [3].
- The maximum pressure should not exceed 6 bar (red line on the pressure gage). If the maximum pressure is exceeded, the safety valve is actuated and releases the excess pressure.
- The maximum pressure should not exceed 6 bar (red line on the pressure gage). If the maximum pressure is exceeded, the safety valve is actuated and releases the excess pressure.
- Press the pump handle downward and turn it counterclockwise.
- The pump handle is locked.
- The pump handle is locked.
Use
- Connect the plug-in connector of the water pressure tank with the plug-in nipple [1].
- Actuate the ball valve.
- The liquid supply begins.
- The liquid quantity can be regulated with the ball valve.
- The liquid supply begins.
- Continue pumping if the pressure drops below 1 bar [2].
- When the tank is empty, refill it.
After use
- Pull up the red button of the safety valve until the tank is completely depressurized.
- Close the ball valve and disconnect the plug-in connection and plug-in nipple [1].
- Lock the pump handle.
- Screw the pump out of the tank.
- Drain the remaining water from the tank.
- Wipe off the water supply unit with a damp cloth.
- Coil the hose around the tank and mount the plug-in connection on the locating pin of the water supply unit [2].
- Keep the water supply unit in a dry, frost-free environment protected from direct sunlight for drying and storage.
Care and maintenance
Care and maintenance work
- Check the unit at regular intervals.
- We recommend having an expert conduct an external inspection every 2 years and an internal inspection every 5 years, as well as a strength test every 10 years
- We recommend having an expert conduct an external inspection every 2 years and an internal inspection every 5 years, as well as a strength test every 10 years
- Dismantle the pump [1] and grease the O-ring [a] is and the sleeve [b].
- Always carry out this maintenance after using the unit 50 times, however at least once a year!
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Troubleshooting table
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The water supply unit does not build up any pressure |
Pump is not screwed on tightly |
|
O-ring on the pump is defective |
|
|
Sleeve is defective |
|
|
Liquid escapes from the pump at the top |
Valve disk is dirty or defective |
|
Safety valve vents too early |
Safety valve is defective |
|
Pressure gage indicates no tank pressure |
Pressure gage is defective |
|
Disposal
Do not dispose of this product in household waste!Most of the materials from which Hilti tools, appliances and devices are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti sales representative for further information.
Manufacturer's information
The products HILTI DWP10 of the series 3585 meet the requirements of the Pressure Equipment Directive 2014/68/EU and bear the CE marking.Please contact your local Hilti representative if you have questions about the warranty conditions.